Solution


Bridge Lifting and Positioning

New bridges on construction sites need to be carefully lifted and positioned to their final destination. This requires a load monitoring system in order to improve safety and ensure efficiency of the overall application.


BridgeLiftandPositionGraphic

Summary

  • Customer Need / Challenge

    New bridges on construction sites need to be carefully lifted and positioned to their final destination. This requires a load monitoring system in order to improve safety and ensure efficiency of the overall application.

  • Interface Solution

    Interface suggests installing WTSLP Wireless Stainless Steel Load Pins in the cranes performing the lifting and positioning. Loads are monitored and data is wirelessly transmitted to the customer’s PC through WTS-BS-4 Wireless Base Station with USB Interface in Industrial Enclosure. It can also be transmitted to the WTS-HK-S Next-Generation Wireless Handheld. Data can be displayed, logged, and graphed with supplied Log100 software.

  • Results

    Interface’s WTSLP Wireless Stainless Steel Load Pins paired with Interface’s Wireless Telemetry System was the perfect monitoring system solution for lifting and positioning a bridge.

Materials


  • WTSLP Wireless Stainless Steel Load Pins
  • WTS-BS-4 Wireless Base Station with USB Interface in Industrial Enclosure with included Log100 Software
  • WTS-HK-S Next-Generation Wireless Handheld
  • Customer Laptop

How it Works


  1. WTSLP Wireless Stainless Steel Load Pins are installed into the cranes that will lift the bridge pieces.
  2. The WTSLP Wireless Stainless Steel Load Pins capture the bridge’s load and wirelessly transmits it to the customer’s PC through the WTS-BS-4 Wireless Base Station with USB Interface in Industrial Enclosure.
  3. Customer’s also have the option of using the WTS-HK-S Next-Generation Wireless Handheld. Results are displayed, graphed, and recorded with supplied Log100 software.

Download PDF